Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Liebert GXT5
Lithium-Ion UPS
Firmware Downloads

SIGN UP FOR SOFTWARE UPDATES

Releases for Vertiv Liebert GXT5 Lithium-Ion UPS 1000-3000VA (LV, I)

GXT5LI-1000LVRT2UXL, GXT5LI-1500LVRT2UXL, GXT5LI-2000LVRT2UXL, GXT5LI-3000LVRT2UXL, GXT5LI-1000IRT2UXL, GXT5LI-1500IRT2UXL, GXT5LI-2000IRT2UXL, GXT5LI-3000IRT2UXL


NOTE: Each release includes all the updates from previous releases. If upgrading a firmware version that is several releases old, it is only necessary to install the latest. For detailed instructions refer to the user guide.

RELEASE DATE PRODUCT FAMILY VERSION DOWNLOAD
MCU DSP
June 2025
1000-3kVA (LV, I) V190 V140 GXT5LI (1-3k LVI) 2025-June.zip -

Release Notes:

  1. Start with No Battery ENABLED by default.
  2. Auto Restart without Battery ENABLED by default.
  3. HID re-map.
  4. Power Assist output voltage corrected.
  5. For I models, IT system compatibility is now Enabled.
  6. Battery Test now takes 30 seconds to complete and is performed by the BMS. ND23 event code is added for Battery Test Pass.

Note: To sync GXT5 LI MCU Firmware across all models, GXT5 LI LV/I Firmware has moved directly to V190

August 2024
1000-3kVA (LV, I) V170 V130 GXT5LI (1-3k LV,I) 2024-08.zip -

Release Notes:

  1. Optimized the fan speed control to reduce audible noise levels.
RELEASE DATE PRODUCT FAMILY VERSION DOWNLOAD
MCU DSP BMS
October 2023
1000-3000VA (LV, I) V160 V120 V120 GXT5LI (1-3k LV,I) 2023-Oct.zip -

Release Notes:

  1. Improved RDU101 web-interface active events log by removing "UPS Output on Inverter" alert.
  2. Improved the Lithium battery parameters on the UPS LCD
  3. Enabled the ability to remotely update the BMS firmware through the UPS communication cable
  4. MCU firmware was remerged with the 5-10kVA models (why it skipped from V130 to V160 due to 5-10kVA release of MCUV150)
May 2022
1000-3000VA (LV, I) V130 V120 V110 GXT5LI MCUV130-DSPV120-LV-I 2022-May.zip +


Releases for Vertiv Liebert GXT5 Lithium-Ion UPS 5KVA-10KVA (MV)

GXT5LI-5000MVRT3UXLN, GXT5LI-6000MVRT3UXLN, GXT5LI-8000MVRT4UXLN, GXT5LI-10KMVRT4UXLN


NOTE: Each release includes all the updates from previous releases. If upgrading a firmware version that is several releases old, it is only necessary to install the latest. For detailed instructions refer to the user guide.

RELEASE DATE PRODUCT FAMILY VERSION DOWNLOAD
MCU DSP BMS
May 2025
5kVA-10kVA (MV) V180 V170 GXT5LI (5-10k MV) 2025-May.zip -

Release Notes:

  1. Start with No Battery ENABLED by default.
  2. Auto Restart without Battery ENABLED by default.
  3. HID re-map.
  4. Power Assist output voltage corrected.
  5. Improved DSP Processor auto-reboot process. Unit will now log UPS state and transfer to bypass during DSP reboot.
  6. Soften the transfer from (Internal) Bypass back to operation on inverter.

Note: To sync GXT5 LI MCU Firmware across all models, GXT5 LI MV Firmware has moved directly to V180.

September 2023
5KVA-10KVA (MV) V160 V160 V130 GXT5LI (5-10k MV) 2023-Sept.zip +

August 2022
5KVA-10KVA (MV) V150 V140 V120 GXT5LI (5-10k MV) 2022-Aug.zip +

July 2022
5KVA-10KVA (MV) V130 V130 V110 GXT5LI-MCUV150DSPV140BMSV130(5-10k MLV)(2022-07).zip +

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location